Skip to main content
Ygndz.1
Associate
January 7, 2022
Question

STM32F0 ADC DMA or Not DMA

Hello. I am making software with STM32F030CCT6 processor. I am trying to make ADC with or without DMA. I always face this problem in F0 series. I can read only one channel. When it switches to multi-channel, it transfers data from a single channel to all channels. In the STM32F4 series, we could choose the rank in the settings. So it was easy to run DMA. You can't choose rank on this one. How to read multiple ADCs in F0 series Can you help with the HAL library?

This topic has been closed for replies.

3 replies

Ygndz.1
Ygndz.1Author
Associate
January 7, 2022

Guys, I found the solution. Stuck friends can try the code here.

https://community.st.com/s/feed/0D50X0000BDmUYOSQ3

TDK
January 7, 2022

The ADC peripheral varies between series, so don't expect the interface to be the same. It's also perhaps the peripheral with the most examples.

Here is an example on the F0 for reading multiple ADC channels.

https://github.com/STMicroelectronics/STM32CubeF0/blob/4390ff6bfb693104cf97192f98c3dc9e3a7c296a/Projects/STM32F072RB-Nucleo/Examples/ADC/ADC_Sequencer/Src/main.c

"If you feel a post has answered your question, please click ""Accept as Solution""."
Muhammed Güler
Senior III
January 7, 2022

In the F0 series, you can only scan from first to last or from last to first. If you are using 2, 5, 7 inputs, you can only read 2-5-7 or 7-5-2. default order 2-5-7