Skip to main content
mikael239955_stm1
Associate
March 21, 2013
Question

STM32F USB Firmware (cdc class driver) bug (64 byte transfers from device to host)

  • March 21, 2013
  • 2 replies
  • 943 views
Posted on March 21, 2013 at 10:46

Hi,

64 byte transfers from my STM32F4 cdc driver to the host side fails. 63 bytes work, as well as 65 bytes.

A quick forum search indicates that this is a bug in the cdc class driver firmware. A 64 byte transfer should be followed by a 0-byte transfer so that the host side (windows) can detect end of transfer. So, this bug is known but I have so far failed to find a fix for it. Does anyone know how to fix it - or is there a firmware library out there somewhere where this is fixed already?

Currently I'm using

''STM32_USB-Host-Device_Lib_V2.1.0'', V1.1.0 / 19-March-2012

Best regards,

Mikael
    This topic has been closed for replies.

    2 replies

    tyronexj
    Visitor II
    March 22, 2013
    Posted on March 22, 2013 at 10:04

    Hi Mikael,

    I am working with USB VCP example recently.

    I am not sure whether following modification could fix the bug.

    /**

      * @brief  Handle_USBAsynchXfer

      *         Send data to USB

      * @param  pdev: instance

      * @retval None

      */

    static void Handle_USBAsynchXfer (void *pdev)

    {

      uint16_t USB_Tx_ptr;

      static uint16_t USB_Tx_length = 0;

     

      if(USB_Tx_State != 1)

      {

        if (APP_Rx_ptr_out == APP_RX_DATA_SIZE)

        {

          APP_Rx_ptr_out = 0;

        }

        

        if(APP_Rx_ptr_out == APP_Rx_ptr_in)

        {

          if(USB_Tx_length == CDC_DATA_MAX_PACKET_SIZE)

          {

            USB_Tx_length = 0;

          }

          else

          {

            USB_Tx_length = 0;

            USB_Tx_State = 0;

            return;

          }

        }

        else if(APP_Rx_ptr_out > APP_Rx_ptr_in) /* rollback */

        {

          APP_Rx_length = APP_RX_DATA_SIZE - APP_Rx_ptr_out;

        

        }

        else

        {

          APP_Rx_length = APP_Rx_ptr_in - APP_Rx_ptr_out;

         

        }

    #ifdef USB_OTG_HS_INTERNAL_DMA_ENABLED

         APP_Rx_length &= ~0x03;

    #endif /* USB_OTG_HS_INTERNAL_DMA_ENABLED */

        if (APP_Rx_length > CDC_DATA_IN_PACKET_SIZE)

        {

          USB_Tx_ptr = APP_Rx_ptr_out;

          USB_Tx_length = CDC_DATA_IN_PACKET_SIZE;

          

          APP_Rx_ptr_out += CDC_DATA_IN_PACKET_SIZE;

          APP_Rx_length -= CDC_DATA_IN_PACKET_SIZE;

        }

        else

        {

          USB_Tx_ptr = APP_Rx_ptr_out;

          USB_Tx_length = APP_Rx_length;

          

          APP_Rx_ptr_out += APP_Rx_length;

          APP_Rx_length = 0;

        }

        USB_Tx_State = 1;

        DCD_EP_Tx (pdev,

                   CDC_IN_EP,

                   (uint8_t*)&APP_Rx_Buffer[USB_Tx_ptr],

                   USB_Tx_length);

      }

    }

    Best regards,

    Tyrone

    tyronexj
    Visitor II
    March 22, 2013
    Posted on March 22, 2013 at 10:58

    Sorry,

    usbd_cdc_DataIn() also calls DCD_EP_Tx(CDC_IN_EP), then static uint16_t USB_Tx_length = 0 should be seen in the whole file.

    Best regards,

    Tyrone