Skip to main content
astrid
Associate II
November 9, 2015
Question

STM32CubeMXF1 HAL_Driver vs Standard Peripheral lib papal schism?

  • November 9, 2015
  • 3 replies
  • 898 views
Posted on November 10, 2015 at 00:26

Disclose any of insiders as it will integrate STM32Cube and new HAL Drivers to the Keil MDK-ARM and his Software pack for STM32Fx?Recently released sw pack STM32F1xxDPF v 2.0.0 for MDK-ARM building on Standard Peripheral lib v3.5.0 and CMSIS OS RTX .STM32CubeMX include new HAL_Driver and FreeRTOS. Thanks to this ''papal schism'' is difficult for exaple use in project generated witch STM32Cube any sw component from MDK Middleware. Whereas a year ago it spoke about closer integration STM32Cube into sw packt for MDK-ARM.May I ask what is planned in this field and when?

See last section in

http://www.keil.com/appnotes/files/apnt_266.pdf

    This topic has been closed for replies.

    3 replies

    Andrei Chichak
    Lead
    November 10, 2015
    Posted on November 10, 2015 at 01:43

    Words. Many words. Some of them I even recognize. Communication of a coherent idea? Not so much.

    Was this a google translation from another language? Perhaps you could post your question in the original language and a native speaker could  answer you.
    astrid
    astridAuthor
    Associate II
    November 17, 2015
    Posted on November 17, 2015 at 19:01

    OK

    One should not

    go into

    philosophical

    debates

    in

    language

    that can not

    well

    .

    My English

    is very poor

    .

    Plus

    I have

    typos

    in the text

    ,  with / wich

    Simplify

    query

    .

    In yar 2014 I read

    At the same time, we plan to integrate STM32CubeMX and Keil MDK such that the code generated by STM32CubeMX will be used to configure the drivers. This will greatly simplify device and driver configuration and provide more robust configurations and drivers.

    See

    the last

    http://www.keil.com/appnotes/files/apnt_266.pdf

    Now is

    the end of the year

    2015 and last Software pack for MDK-ARM 5.17, for example v2.0.0 STM32F1 use old STM32F10x Standard Peripherals Library v 3.5.0.

    STMCube32 use new HAL driver for examéle STM32F1 v1,2

    I do not know

    ,

    for me it

    is not

    much

    integration

    , for me it is Papal schism!

    I'm interested in

    further

    development

    ?

    He plans to

    move to

    the new HAL (CubeMX

    )

    of the library

    in the

    software

    pack

    for

    MDK

    -

    ARM

    ?

    Tesla DeLorean
    Guru
    November 17, 2015
    Posted on November 17, 2015 at 19:18

    May be you're in the wrong church? These questions about when Keil might do things would be better addressed to Keil, no?

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..