STM32CUBEMX with Discovery F411VE
Hello after installing the latest version of CUBEMX(4.27) and generating a default project for my STM32F411VE Discovery board by choosing the option to initialize all the peripherals in their default mode it ended up not working. After some debugging I've come to the conclusion that it enters a failure while(1) loop in the SystemClock_Config function and more specifically at :
RCC_OscInitTypeDef RCC_OscInitStruct;
RCC_ClkInitTypeDef RCC_ClkInitStruct;
RCC_PeriphCLKInitTypeDef PeriphClkInitStruct;
/**Configure the main internal regulator output voltage
*/
__HAL_RCC_PWR_CLK_ENABLE();
__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);
/**Initializes the CPU, AHB and APB busses clocks
*/
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;
RCC_OscInitStruct.HSEState = RCC_HSE_BYPASS;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
RCC_OscInitStruct.PLL.PLLM = 4;
RCC_OscInitStruct.PLL.PLLN = 192;
RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV4;
RCC_OscInitStruct.PLL.PLLQ = 8;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__); /* <==============HERE */
}
After further investigation of HAL_RCC_OscConfig
I've found that it returns HAL_TIMEOUT and more specifically in this section of code.
/* Check the HSE State */
if((RCC_OscInitStruct->HSEState) != RCC_HSE_OFF)
{
/* Get Start Tick*/
tickstart = HAL_GetTick();
/* Wait till HSE is ready */
while(__HAL_RCC_GET_FLAG(RCC_FLAG_HSERDY) == RESET)
{
if((HAL_GetTick() - tickstart ) > HSE_TIMEOUT_VALUE)
{
return HAL_TIMEOUT;
}
}
}
I've tried disabling some peripherals and nothing seems to work. Since I haven't really done anything special with the CODEMX generation (just chose the board and set up FreeRTOS with a systick of TIM11) I'm thinking it can only be a bug. And in my case it's a show stopper. I'd love some assistance.
Thank you in advance.