Question
STM32CubeMX v2.25 Bug Report ''SW4STM32Project generation have a problem''
Posted on April 09, 2018 at 10:05
I have a pretty simple project and at some point I got this error when generating code:
The Code is successfully generated under ...
but SW4STM32Project generation have a problem
In the console I have this error:
2018-04-09 09:37:48,072 [INFO] UtilMem:74 - End SaveConfig() Used Memory: 203881040 Bytes (775421952)
2018-04-09 09:37:48,098 [INFO] ProjectBuilder:299 - [PM] Start Project Generation Thread2018-04-09 09:37:48,211 [INFO] BlockDiagram:1141 - set Specific Code input for plugin: ADC2018-04-09 09:37:48,211 [INFO] BlockDiagram:1141 - set Specific Code input for plugin: SPI2018-04-09 09:37:48,211 [INFO] BlockDiagram:1141 - set Specific Code input for plugin: NVIC2018-04-09 09:37:48,212 [INFO] BlockDiagram:1141 - set Specific Code input for plugin: SYS2018-04-09 09:37:48,212 [INFO] BlockDiagram:1141 - set Specific Code input for plugin: I2C2018-04-09 09:37:48,942 [INFO] CodeGenerator:499 - code generatio: config db path: /opt/STM32CubeMX//db/2018-04-09 09:37:49,068 [INFO] CodeEngine:181 - oldGeneratedFile, /temp/Src/license.tmp_save2018-04-09 09:37:49,594 [INFO] CodeEngine:199 - Generated code: /temp/Src/license.tmp2018-04-09 09:37:49,783 [INFO] CodeEngine:181 - oldGeneratedFile, /temp/Src/gpio.tmp_save2018-04-09 09:37:49,958 [INFO] CodeEngine:199 - Generated code: /temp/Src/gpio.tmpCommand lineDebug : prepare data for ADCCommand line testCommand lineDebug : prepare data for I2CCommand line testCommand lineDebug : prepare data for SPICommand line testCommand lineDebug : prepare data for SYSCommand line testDebug : prepare data for NVICCommand line test2018-04-09 09:37:50,266 [INFO] CodeEngine:181 - oldGeneratedFile, /temp/Src/stm32l0xx_it.c_save2018-04-09 09:37:50,371 [INFO] CodeEngine:199 - Generated code: /temp/Src/stm32l0xx_it.c2018-04-09 09:37:50,378 [INFO] CodeEngine:181 - oldGeneratedFile, /temp/Inc/stm32l0xx_it.h_save2018-04-09 09:37:50,451 [INFO] CodeEngine:199 - Generated code: /temp/Inc/stm32l0xx_it.h2018-04-09 09:37:50,474 [INFO] CodeEngine:181 - oldGeneratedFile, /temp/Src/stm32l0xx_hal_msp.c_save2018-04-09 09:37:50,624 [INFO] CodeEngine:199 - Generated code: /temp/Src/stm32l0xx_hal_msp.c2018-04-09 09:37:50,627 [INFO] CodeEngine:181 - oldGeneratedFile, /temp/Src/system.tmp_save2018-04-09 09:37:50,698 [INFO] CodeEngine:199 - Generated code: /temp/Src/system.tmp2018-04-09 09:37:50,705 [INFO] CodeEngine:181 - oldGeneratedFile, /temp/Inc/stm32l0xx_hal_conf.h_save2018-04-09 09:37:50,851 [INFO] CodeEngine:199 - Generated code: /temp/Inc/stm32l0xx_hal_conf.h2018-04-09 09:37:50,869 [INFO] CodeEngine:181 - oldGeneratedFile, /temp/Inc/main.h_save2018-04-09 09:37:51,005 [INFO] CodeEngine:199 - Generated code: /temp/Inc/main.h2018-04-09 09:37:51,009 [INFO] CodeEngine:181 - oldGeneratedFile, /temp/Src/main.c_save2018-04-09 09:37:51,129 [INFO] CodeEngine:199 - Generated code: /temp/Src/main.c2018-04-09 09:37:51,345 [INFO] ProjectBuilder:1260 - Time for Copy HAL[1] : 35mS.2018-04-09 09:37:51,359 [INFO] ProjectBuilder:1723 - Project Generator version: 2.27.02018-04-09 09:37:51,379 [INFO] ConfigFileManager:451 - The Die is : DIE4172018-04-09 09:37:52,838 [INFO] ToolchainGenerator:125 - stack trace : java.io.FileNotFoundException: /temp/custom.xml (Datei oder Verzeichnis nicht gefunden) at java.io.FileInputStream.open0(Native Method) at java.io.FileInputStream.open(FileInputStream.java:195) at java.io.FileInputStream.<init>(FileInputStream.java:138) at java.io.FileInputStream.<init>(FileInputStream.java:93) at generators.SysWbgenerator.setDebugOptions(SysWbgenerator.java:2329) at convertor.Convertor.generateSW4STM32Project(Convertor.java:1466) at convertor.Convertor.generateSw4STM32Files(Convertor.java:1311) at convertor.Convertor.generate(Convertor.java:659) at convertor.Convertor.convert(Convertor.java:559) at convertor.Convertor.updateProject(Convertor.java:412) at com.st.microxplorer.plugins.projectmanager.model.ToolchainGenerator.update(ToolchainGenerator.java:119) at com.st.microxplorer.plugins.projectmanager.engine.ProjectBuilder.createToolChainFolders(ProjectBuilder.java:1776) at com.st.microxplorer.plugins.projectmanager.engine.ProjectBuilder.createProject(ProjectBuilder.java:595) at com.st.microxplorer.plugins.projectmanager.engine.GenerateProjectThread.run(GenerateProjectThread.java:41)2018-04-09 09:37:52,839 [INFO] ToolchainGenerator:126 - [Project Generator] Problem in the update of the project
2018-04-09 09:37:52,839 [INFO] ProjectBuilder:1785 - Time for Generating toolchain IDE Files: 1484mS.2018-04-09 09:37:52,839 [ERROR] ProjectBuilder:1791 - Error in Project Generation2018-04-09 09:37:52,839 [ERROR] ProjectBuilder:611 - Error in Project GenerationWhat's wrong here?