Skip to main content
Tim Michals
Associate II
Jul 6, 2016 2:22 PM UTC
Solved

stm32cubemx Ubuntu 16.04 LTS 64 Bit crash

Posted on July 06, 2016 at 16:22

Running the install SetupSTM32CubeMX-4.15.1.linux

crashes. 

OS: Ubuntu 16.04LTS 64 Bit

java version:

java -version

openjdk version ''9-internal''

OpenJDK Runtime Environment (build 9-internal+0-2016-04-14-195246.buildd.src)

OpenJDK 64-Bit Server VM (build 9-internal+0-2016-04-14-195246.buildd.src, mixed mode)

Attached is crash log

    This topic has been closed for replies.
    Tim Michals
    Tim MichalsBest answer
    Associate II
    May 19, 2017 1:04 AM UTC
    Posted on May 19, 2017 at 01:04

    Yes, it does.  Thank you issue resolved.

    6 replies

    Nesrine M_O
    Associate
    Jul 13, 2016 1:07 PM UTC
    Posted on July 13, 2016 at 15:07

    Hi michals.tim,

    I have an issue to open your crash log.Could you please reattach it? 

    -Syrine-

    rchrdlyon1
    Associate II
    Jul 14, 2016 3:09 PM UTC
    Posted on July 14, 2016 at 17:09

    I have a similar problem with the same operating system. When I try:

    cd to directory where the file SetupSTM32CubeMX-4.15.1.linux is located

    $ sudo ./SetupSTM32CubeMX-4.15.1.linux

    The installer runs but always generates the following message:

    sudo: unable to execute ./SetupSTM32CubeMX-4.15.1.linux: No such file or directory

    Tried the default openjdk as well as oracle java.

    The last version of of the installer that worked was SetupSTM32CubeMX-4.13.0.linux with oracle java. Later versions do not. Hopefully one day this problem will resolved.

    Regards ...

    rchrdlyon1
    Associate II
    Jul 14, 2016 4:22 PM UTC
    Posted on July 14, 2016 at 18:22

    sudo java -jar SetupSTM32CubeMX-4.15.1.exe -console

    seems to work. STM32CubeMX is working on default openjdk supplied with ubuntu.

    stm32cube-t
    ST Employee
    Jul 21, 2016 10:11 AM UTC
    Posted on July 21, 2016 at 12:11

    Dear all,

    We do not reproduce your issue.

    Please note STM32CubeMX on Linux is a 32 bit application. Do you confirm that you have 32 bit compliant packages installed on your Linux 64 bit?

    The tool also requires: java 1.7.0_45 or later.

    Best regards 

    ST Employee
    Feb 2, 2017 11:05 AM UTC
    Posted on February 02, 2017 at 12:05

    Hello All,

    CubeMX-4.19 with oracle java version 1.8.0_121, on Ubuntu 64 bits has been tested.

    IT works well.

    I was able to install, launch and creates a project.

    Has this thread was long ago, I guess everything has been fixed since.

    Kind regards

    Sirma

    Tim Michals
    Tim MichalsAuthorBest answer
    Associate II
    May 19, 2017 1:04 AM UTC
    Posted on May 19, 2017 at 01:04

    Yes, it does.  Thank you issue resolved.