Skip to main content
Asantos
Associate III
September 9, 2014
Question

STM32CubeMx STM32F3 CCM-RAM

  • September 9, 2014
  • 1 reply
  • 475 views
Posted on September 10, 2014 at 00:31

Hi,

  I would like to know if there are the option to create a IAR project in the STM32CubeMx that use CCM-RAM to run interrupt routines. If not. Are there plans to add it in the future?

Ari.
    This topic has been closed for replies.

    1 reply

    stm32cube-t
    ST Employee
    October 6, 2014
    Posted on October 06, 2014 at 16:36

    Hello,

    STM32CubeMX does not support this specification configuration.

    A manual update is required instead (refer to the application note:

    http://www.st.com/web/en/resource/technical/document/application_note/DM00083249.pdf

    ).

     

    We'll log your request as a possible enhancement for CubeMX.

    Thank you.