Skip to main content
Elwood Downey
Associate III
Feb 9, 2017 7:12 PM UTC
Question

STM32CubeMX import bug?

Posted on February 09, 2017 at 20:12

Hello all,

I am using STM32CubeMX Version 4.19.0. I developed my project using Nucleo F446ZE which uses the LQFP package. It's all working great so now I need to move to the deployed package which is the F446ZEH UFBGA. Here is what I did in Cube:

  1. create a New Project
  2. select STM32F446ZEH
  3. File -> Import project
  4. select Import Project settings
  5. browse to my Nucleo project .ioc file and click ok
  6. select Automatic import
  7. click ok
  8. it cranks for a few seconds then says 'Project is successfully imported'
  9. However, in the bottom pane is the following ominous yellow message:
  10. Import :

    Some parameters can't be imported for ADC1

    Can't import parameter:Channel = ADC_CHANNEL_TEMPSENSOR, it isn't a possible value in STM32F446ZEHx, it's set to default value.

    Importing project completed
  11. Moving on anyway, I set up Project -> Settings and then Project -> Generate Code.
  12. I went ahead and did a build and it all compiles and links fine (I'm using gcc).
  13. I can not test it yet but I don't see anything wrong. In particular I diff'd all source files between the two projects that contain 

    ADC_CHANNEL_TEMPSENSOR and they are identical.

So I can't be sure, but I'm more inclined to think this warning from Cube is bogus. Any confirmation of that, either way, would be appreciated.

Thanks for reading.

    This topic has been closed for replies.

    1 reply

    Nesrine M_O
    Associate
    Feb 13, 2017 9:41 AM UTC
    Posted on February 13, 2017 at 10:41

    Hi

    Downey.Elwood

    ,

    Please follow steps in the

    /external-link.jspa?url=http%3A%2F%2Fwww.st.com%2Fcontent%2Fccc%2Fresource%2Ftechnical%2Fdocument%2Fuser_manual%2F10%2Fc5%2F1a%2F43%2F3a%2F70%2F43%2F7d%2FDM001047pdf%2Ffiles%2FDM001047pdf%2Fjcr%3Acontent%2Ftranslations%2Fen.DM001047pdf

    ,Tutorial 5:

    exporting current project configuration to a compatible MCU

    ,then tell us about the result.

    -Nesrine-