Skip to main content
GnR
Associate II
September 13, 2017
Question

STM32CubeMX FATFS + USB-MSD

  • September 13, 2017
  • 0 replies
  • 738 views
Posted on September 13, 2017 at 21:23

I’m trying to implement a simple data-logger that runs on a bespoke STM32F2xx board which is capable of storing data to an SD-Card (SDIO 4-bit + DMA) and will enable windows to copy the stored data from the SD-Card using USB-MSD.

I do not intend for the data-logger and the USB-MSD to have access the SD-Card at the same time but rather use a GPIO input to select how the device boots i.e data-logger or USB-MSD mode.

Using STM32FCubeMX (V4.22.0) and SW4STM32 I have separately developed the data-logger (FATFS based) and the USB_MSD (MSC based) which have both been proven function.

My problem occurs when I try to combine the data-logger and USB-MSD which results in a USB-MSD failure as windows reports that the removable disk (USB-MSD) requires formatting. This problem only occurs when FATFS (SD-Card) is enabled within STM32CubeMX.

I have tried various methods of implementing FATFS without unduly effecting the operation of USB-MSD but all this has resulted in is more confusion on my part.

 

I would be grateful if anyone could advise me how I can implement the above i.e. a system that will boot as either a data-logger or USB-MSD dependant on the state of a GPIO input.

    This topic has been closed for replies.