Skip to main content
jackbauer007
Associate
June 30, 2016
Question

STM32CubeMX + FatFS - Keil works, TrueStudio not

  • June 30, 2016
  • 5 replies
  • 1058 views
Posted on June 30, 2016 at 13:02

Hello my friends,

I am new to FatFs and I want to write something on the SD-Card. I initialize SDIO and FatFs over STM32CubeMX. I am using the STM32F4 Discovery and the Baseboard which has a SD-Connector. If I create the project for Keil I can write to the SD-Card. But if I create the project for Truestudio or SW4STM32 I can not write to SD-Card.

/* USER CODE BEGIN 2 */
MX_FATFS_Init();
if (f_mount(&SDFatFs, (TCHAR const*) SD_Path, 0) != FR_OK) {
/* FatFs Initialization Error */
Error_Handler();
}
if (f_open(&MyFile, ''STMTXT'', FA_CREATE_ALWAYS | FA_WRITE) != FR_OK) {
Error_Handler();
}
res = f_write(&MyFile, wtext, sizeof(wtext), (void *) &byteswritten);
if ((byteswritten == 0) || (res != FR_OK)) {
Error_Handler();
}
f_close(&MyFile);
/* USER CODE END 2 */

I put exact the same Code in to all three projects but only Keil works. It is not a compilation error. Mount works too but always get stucked in f_open. I have noticed thatHAL_SD_ReadBlocks returns an Error. I have created multiple project with FreeRTOS and without. Always works in Keil but not with Truestudio and SW4STM Does somebody know what I am doing wrong? Best Regards, Kevin #!stm32-!fatfs-!keil-!truestudio
    This topic has been closed for replies.

    5 replies

    slimen
    Visitor II
    June 30, 2016
    Posted on June 30, 2016 at 13:38

    Hi,

    Could you please precise which version of HAL, STM32CubeMx and toolchain are you using?

    Regards

    jackbauer007
    Associate
    June 30, 2016
    Posted on June 30, 2016 at 13:47

    Hello,

    sorry that I have not noticed it.

    I am using STM32CubeMX v4.15.1 and Firmware Package 1.12.0

    TrueStudio 5.5.2 

    SW4STM32 v1.8 from May 4, 2016.

    Keil 5.17

    Best Regards

    Kevin
    Tesla DeLorean
    Guru
    June 30, 2016
    Posted on June 30, 2016 at 14:39

    How about SDIO and DMA interrupt handlers?

    Not compiler error/failure? You sure? Does behaviour change with optimization off vs on? Check also statics are being cleared.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    slimen
    Visitor II
    June 30, 2016
    Posted on June 30, 2016 at 15:22

    Hi lange.kevin, 

    It's better to compare your generated code with one of the provided FatFS applications  working with SD-Card, as this example:

    STM32Cube_FW_F4_V1.12.0\Projects\STM32F412G-Discovery\Applications\FatFs\FatFs_uSD

    Regards

    jackbauer007
    Associate
    July 1, 2016
    Posted on July 01, 2016 at 13:28

    Thank you guys. You got me in the right direction. 

    I have made mistakes with DMA.

    Sometimes you need to talk to somebody to solve the obvious mistakes.