Skip to main content
john doe
Senior III
August 9, 2017
Question

STM32CubeMX bug - can't select AF on PH6

  • August 9, 2017
  • 0 replies
  • 745 views
Posted on August 09, 2017 at 03:39

STM32CubeMX 4.22.0, F7 cube 1.7, stm32f769i-discovery

I want a 32 bit timer with pwm capture on the arduino headers. Attempting to select TIM2_CH1 on  PH6 fails. In the application, it just puts the ball to reset mode and puts PA5 to the AF for TIM2_CH1. PA5 doesn't reach the headers so its of no use to me.

The card that comes with the board says that PH6 is D9 not D6. for what its worth.

0690X00000607l8QAA.png
    This topic has been closed for replies.