Skip to main content
Eugene S.
Associate III
Dec 24, 2016 2:15 PM UTC
Solved

STM32CubeMX bad macro generation (bug)

Posted on December 24, 2016 at 15:15

I use STM32CubeMX v4.0. It generates MX_Device.h file for configuring CMSIS-Drivers. I found that there are some macroses use hyphen symbol, which is not allowed:

/*-------------------------------- SYS --------------------------------*/
#define MX_SYS 1
/* GPIO Configuration */
/* Pin PE2 */
#define MX_SYS_TRACECLK_Pin PE2
#define MX_TRACECLK SYS_TRACECLK
/* Pin PA13 */
#define MX_SYS_JTMS-SWDIO_Pin PA13
#define MX_SWDIO SYS_JTMS-SWDIO
/* Pin PE3 */
#define MX_SYS_TRACED0_Pin PE3
#define MX_TRACED0 SYS_TRACED0
/* Pin PA14 */
#define MX_SYS_JTCK-SWCLK_Pin PA14
#define MX_SWCLK SYS_JTCK-SWCLK
/* Pin PE6 */
#define MX_SYS_TRACED3_Pin PE6
#define MX_TRACED3 SYS_TRACED3
/* Pin PE4 */
#define MX_SYS_TRACED1_Pin PE4
#define MX_TRACED1 SYS_TRACED1
/* Pin PE5 */
#define MX_SYS_TRACED2_Pin PE5
#define MX_TRACED2 SYS_TRACED2�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?

    This topic has been closed for replies.
    Sirma Siang
    Sirma SiangBest answer
    ST Employee
    Sep 13, 2017 10:55 AM UTC
    Posted on September 13, 2017 at 10:55

    Hello

    ,

    Great thanks for your inputs.

    I am able to reproduce it at my end.

    The point is that MX_Device.h is generated by Cube, based on a ftl template coming from ARM.

    You can find it in the F4 package, downloaded from ARM, here:

    C:\Keil_v5\ARM\PACK\Keil\STM32F4xx_DFP\2.0\MDK\CubeMX

    Waiting for ARM correction, you can replace the MX_Device_h.ftl template by the one I upload.

    Thus, we are submitting a ticket to ARM.

    Hope it help you

    Kind regards

    Sirma

    ________________

    Attachments :

    MX_Device_h.ftl.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HyS0&d=%2Fa%2F0X0000000b7n%2F6sgeMKvFhVLLcheml9DYPVOMO1SYMLEiz071VjoOBAo&asPdf=false

    6 replies

    Seb
    ST Employee
    Dec 24, 2016 3:01 PM UTC
    Posted on December 24, 2016 at 16:01

    Hi Eugene,

    I've passed your note to the CubeMX team.

    Thanks!

    Eugene S.
    Eugene S.Author
    Associate III
    Apr 9, 2017 10:24 AM UTC
    Posted on April 09, 2017 at 12:24

    Hi

    marsanne.sebastien

    ,

    Do you have any plans to fix the bug?

    The bug still exists in v 4.1

    Sirma Siang
    ST Employee
    Sep 12, 2017 6:18 PM UTC
    Posted on September 12, 2017 at 18:18

    Hello

    Yauhen.Sinkevich

    ;

    Could you please let me know on which family you have observed this error ?

    Great thanks in advance.

    Kind regards

    Sirma

    Eugene S.
    Eugene S.Author
    Associate III
    Sep 12, 2017 6:21 PM UTC
    Posted on September 12, 2017 at 18:21

    Hello

    SIRY.Marc

    ,

    It is STM32F4

    Best regards,

    Eugene.