Skip to main content
David Fisher
Associate II
November 30, 2017
Question

STM32CubeMX 4.23.0 project settings dialog, can't select OK in Ubuntu 17.10

  • November 30, 2017
  • 2 replies
  • 955 views
Posted on November 30, 2017 at 17:32

I am having the same issue with STM32CubeMX 4.23.0 that I had with the previous version. Having upgraded to Ubuntu 17.10 I can't select the ok button to set my Project settings in CubeMX. Any ideas on how I can select the ok button, key combinations etc ? I have tried resolution changes different ways to scroll but nothing works. Could the designers of Cubemx please make the project settings dialog of future versions resizable ?

    This topic has been closed for replies.

    2 replies

    ST Technical Moderator
    December 18, 2017
    Posted on December 18, 2017 at 18:48

    Hello,

    Have you used the Zoom feature (available from the toolbar) ? or tried <CTRL> + Mousewheel to Zoom in or out?

    Best Regards

    Imen

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
    David Fisher
    Associate II
    December 18, 2017
    Posted on December 18, 2017 at 19:38

    <CTRL> + Mousewheel to Zoom in or out

    Doesn't do anything in the project settings dialog and zooming in the

    project window has no effect on the project settings dialog.

    >Have you used the Zoom feature (available from the toolbar) ?

    Isn't available in the Project settings dialog.

    Thanks for trying any other ideas welcome.

    Regards,

    David