Skip to main content
Bogdan Golab
Lead
Jan 20, 2016 9:16 AM UTC
Solved

STM32CubeMX 4.14.0/4.15.0 BUG: Target/IROM settings are NOT preserved

Posted on January 20, 2016 at 10:16

Hi,

Whenever I regenerate the code using STM32CubeMX the new (re-generated) Keil project has Target/IROM1 Memory Areas overwritten  e.g.

I usually use RAM area are for IROM1 for debug purposes

and the IROM1 is set to:

Start: 0x20000000, size:0x1000

After regenerating the code the

IROM1 settings are overwritten and  now I see:

Start: 0x8000000, size:0x10000

Is there any way to make STM32Cube preserve Keil Target/IROM settings?

Please note Target/IRAM settings are preserved. It looks like a bug.

Bogdan

    This topic has been closed for replies.
    Nesrine M_O
    Nesrine M_OBest answer
    Associate
    Apr 4, 2016 2:43 PM UTC
    Posted on April 04, 2016 at 16:43

    Hi golab.bogdan,

    Thank you for your feedback. The issue has been reported internally.

    -Syrine-

    7 replies

    Bogdan Golab
    Lead
    Apr 3, 2016 8:12 AM UTC
    Posted on April 03, 2016 at 10:12

    The bug is still present in 4.14.0

    Bogdan Golab
    Lead
    Apr 3, 2016 8:13 AM UTC
    Posted on April 03, 2016 at 10:13

    Is there any way to make ST developers aware of this issue?

    Nesrine M_O
    Nesrine M_OBest answer
    Associate
    Apr 4, 2016 2:43 PM UTC
    Posted on April 04, 2016 at 16:43

    Hi golab.bogdan,

    Thank you for your feedback. The issue has been reported internally.

    -Syrine-

    Bogdan Golab
    Lead
    May 23, 2016 10:06 AM UTC
    Posted on May 23, 2016 at 12:06

    Hi Syrine,

    Unfortunately the issue was NOT fixed in the CubeMX 4.15.0. The IROM setting are still altered after re-generating the project using CubeMX.

    Thanks,

    Bogdan

    Bogdan Golab
    Lead
    Nov 7, 2016 4:47 PM UTC
    Posted on November 07, 2016 at 17:47

    Hi,

    I wonder if there any plans to fix the issue. I see the problem also in 4.17.0,

    Bogdan

    Bogdan Golab
    Lead
    Feb 3, 2017 12:50 PM UTC
    Posted on February 03, 2017 at 13:50

    It seems that the issue is fixed at least in 4.19.

    Thank you

    Bogdan

    Alex Ivanov
    Visitor II
    Jun 3, 2017 5:23 AM UTC
    Posted on June 03, 2017 at 07:23

    The same error for STM32F745!!! ver. 4.21.0