Skip to main content
armindavatgaran
Associate III
April 20, 2015
Question

stm32cubef4 camera project for stm324xg_eval board

Posted on April 20, 2015 at 10:50

Hello

According to the page 18 of the ov2640 datasheet(version 1.6), device slave address is 0x60 for write and 0x61 for read, but in the camera_to_usbdisk project, only the write address is defined and used for both read and write operations.

#define CAMERA_I2C_ADDRESS 0x60

Please guide me through this.

Thanks.

    This topic has been closed for replies.

    3 replies

    Tesla DeLorean
    Guru
    April 20, 2015
    Posted on April 20, 2015 at 14:56

    Isn't the low order bit set/cleared deeper into the support code depending if it's a read or write? This is a standard 7-bit I2C addressing mechanism.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    armindavatgaran
    Associate III
    April 20, 2015
    Posted on April 20, 2015 at 15:08

    Do you mean that because of shifting 1 bit to right, the LSB will be excluded ?

    Tesla DeLorean
    Guru
    April 20, 2015
    Posted on April 20, 2015 at 18:14

    Do you mean that because of shifting 1 bit to right, the LSB will be excluded ?

    No, I mean that the bit is controlled deeper in the implementation, 0x60 is the base address. I have no interest digging into the HAL/Cube implementation, but on the SPL side this explicitly handled in the library code.

    /**
    * @brief Transmits the address byte to select the slave device.
    * @param I2Cx: where x can be 1, 2 or 3 to select the I2C peripheral.
    * @param Address: specifies the slave address which will be transmitted
    * @param I2C_Direction: specifies whether the I2C device will be a Transmitter
    * or a Receiver.
    * This parameter can be one of the following values
    * @arg I2C_Direction_Transmitter: Transmitter mode
    * @arg I2C_Direction_Receiver: Receiver mode
    * @retval None.
    */
    void I2C_Send7bitAddress(I2C_TypeDef* I2Cx, uint8_t Address, uint8_t I2C_Direction)
    {
    /* Check the parameters */
    assert_param(IS_I2C_ALL_PERIPH(I2Cx));
    assert_param(IS_I2C_DIRECTION(I2C_Direction));
    /* Test on the direction to set/reset the read/write bit */
    if (I2C_Direction != I2C_Direction_Transmitter)
    {
    /* Set the address bit0 for read */
    Address |= I2C_OAR1_ADD0;
    }
    else
    {
    /* Reset the address bit0 for write */
    Address &= (uint8_t)~((uint8_t)I2C_OAR1_ADD0);
    }
    /* Send the address */
    I2Cx->DR = Address;
    }

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..