Skip to main content
KevinA
Senior
October 6, 2014
Question

STM32Cube Tool Chains

  • October 6, 2014
  • 1 reply
  • 568 views
Posted on October 06, 2014 at 22:18

I downloaded, installed and used your STM32Cube software, Great Stuff, but when it came time to generate the code I was given a choice of :

EWARM IAR 

MDK-ARM Keil 

TrueStudio Atollic 

Tool chains, where is the GNU tool chains?

GNU GCC ARM Tool Chain 

GNU Sourcery CodeBench Lite 

I've been linked to Microchip for 13 years and am looking to move to ARM based MCU's but the one requirement is Open Source and support for new products the SAME year they are released. I purchased your STM32F4 Discovery and was amazed that the cost/performance, that is one of the reason I started looking into ARM based MCU's.

Let me know if there is plans on adding GNU tool chains to STM32Cube, thanks

#atm32cube-tool-chain-gnu-gcc-arm
    This topic has been closed for replies.

    1 reply

    Tesla DeLorean
    Guru
    October 6, 2014
    Posted on October 06, 2014 at 22:39

    Last time I checked Atollic was using some GNU/Eclipse mashup

    It has been suggested to ST at several levels that having Cube generate GNU/GCC makefiles would be a desirable goal, although honestly if it were critically important I'm sure someone could write a script to translate the XML project file into a makefile.

    For the PIC32 one could presumably use the MIPS GNU/GCC compiler
    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..