Skip to main content
Duggan.Robert
Associate II
June 27, 2018
Question

STM32Cube MX Project Build Problem

Posted on June 27, 2018 at 17:03

STM32Cube MX Project Build Problem

I'm having a build problem with a project brought over from STM32CubeMX with a -F072RB chip.

After opening the project in True Studio and building (clean) I find the following error (with description):Description Resource Path Location Type

expected identifier or '(' before 'do' stm32f0xx_hal_rcc_ex.h /CAN-PRO M0/Drivers/STM32F0xx_HAL_Driver/Inc line 1203 C/C++ Problem

expected identifier or '(' before 'while' stm32f0xx_hal_rcc_ex.h /CAN-PRO M0/Drivers/STM32F0xx_HAL_Driver/Inc line 1209 C/C++ Problem

in expansion of macro '__HAL_RCC_CAN1_CLK_ENABLE' main.c /CAN-PRO M0/Src line 75 C/C++ ProblemHere is the macro in question:

#define __HAL_RCC_CAN1_CLK_ENABLE() do { \

__IO uint32_t tmpreg; \

SET_BIT(RCC->APB1ENR, RCC_APB1ENR_CANEN);\

/* Delay after an RCC peripheral clock enabling */ \

tmpreg = READ_BIT(RCC->APB1ENR, RCC_APB1ENR_CANEN);\

UNUSED(tmpreg); \

} while(0U)

Any explanation would be helpful.

Thanks, rwduggan
    This topic has been closed for replies.