Skip to main content
cj blades
Associate II
Feb 1, 2017 9:47 PM UTC
Question

STM32Cube doesnt allow HARD_INPUT for SPI slave

Posted on February 01, 2017 at 22:47

Setting up SPI1 as a slave using STM32CubeMx 4.19.0

On the pinout tab of STM32Cube, I can configure SPI1 as Full-Duplex Slave and choose HardwareNSS_Input 

But on the configuration tab , selecting SPI1 configuration , there is a pull down for  'NSS Signal Type' that only allows me to select 'Software' and not 'Hard_Input'

The code that is generated sets it to SPI_NSS_SOFT

Is the tool broken or did I miss some configuration?

I think this worked correctly back in 4.13

    This topic has been closed for replies.