Question
STM3240G-EVAL / STM32F407 / CAN2 Issue
Posted on February 26, 2015 at 17:09
Hello everybody,
I am working with a STM3240G-EVAL card (STM32F407) and I have CAN2 issue, especially the with the reception part. I need help.I already tested the CAN1 channel and it worked really fine. Then I changed the definitions in order to use the CAN2 channel as followed:&sharpdefine
CANx CAN2//CAN1
//CAN1 Clock must absolutely be enabled to use CAN2 !!!
&sharpdefine
CANx_CLK_ENABLE() __HAL_RCC_CAN1_CLK_ENABLE(); __HAL_RCC_CAN2_CLK_ENABLE()&sharpdefine
CANx_GPIO_CLK_ENABLE() __HAL_RCC_GPIOB_CLK_ENABLE()//__HAL_RCC_GPIOD_CLK_ENABLE()
&sharpdefine
CANx_FORCE_RESET() __HAL_RCC_CAN2_FORCE_RESET()//__HAL_RCC_CAN1_FORCE_RESET()
&sharpdefine
CANx_RELEASE_RESET() __HAL_RCC_CAN2_RELEASE_RESET()//__HAL_RCC_CAN1_RELEASE_RESET()
/* Definition for USARTx Pins */
&sharpdefine
CANx_TX_PIN GPIO_PIN_13//GPIO_PIN_1
&sharpdefine
CANx_TX_GPIO_PORT GPIOB//GPIOD
&sharpdefine
CANx_TX_AF GPIO_AF9_CAN2//GPIO_AF9_CAN1
&sharpdefine
CANx_RX_PIN GPIO_PIN_5//GPIO_PIN_0
&sharpdefine
CANx_RX_GPIO_PORT GPIOB//GPIOD
&sharpdefine
CANx_RX_AF GPIO_AF9_CAN2//GPIO_AF9_CAN1
/* Definition for USARTx's NVIC */
&sharpdefine
CANx_RX_IRQn CAN2_RX0_IRQn//CAN1_RX0_IRQn
&sharpdefine
CANx_RX_IRQHandler CAN2_RX0_IRQHandler//CAN1_RX0_IRQHandler
The emission from CAN2 works really fine, but the reception doesn�t. Whatever I send from the other side, the CAN2 Rx buffers stay empty and I don�t have any more ideas.Does that case already happened with somebody else? #stm3240-stm32f407-can2 #can2-configuration #can2-filter-configuration