Question
STM3221G-EVAL : working with rs-232
Posted on November 29, 2012 at 11:54
Hi All ,
I am working with STM3221G-EVAL board, i loaded the STM32F2-F4_Demonstration fw ,that came with the board ,i am trying to work with RS-232 , for now using this fw. when i am trying to type on the LCD and send something back to my pc,it does nothing at all,the settings of the hyperterminal and the settings of the board are identical. the jumper (jp22) is set to rs232 as instructed in the manual. what am i missing? what else should i configure ?any other jumper or something? if there is any other example that relevant only for configuring rs232 and sending data ,it will be mostly appreciated . Thanks Michael #rs-232