Skip to main content
ahmedzizou690
Associate III
May 31, 2014
Question

STM3221G-EVAL ETHERNET

  • May 31, 2014
  • 11 replies
  • 1771 views
Posted on May 31, 2014 at 16:51

I'm a student of University of Tunisia and I'm using IAR Embedded Workbench for ARM, v. 7.10, 32K Kickstart Edition on WIndows 7...

I am

currently

alternating

,

and my

first

project is to

establish communication between

my computer

and

STM3221g-eval

ethernet

connection

.

 

I

focused on creating

blocks

of the function that

will allow

to transform

a file request

by my client

(web

browser)

on appeal from

subroutine.

#!rocketscience
    This topic has been closed for replies.

    11 replies

    ahmedzizou690
    Associate III
    June 3, 2014
    Posted on June 03, 2014 at 16:34

    I'm trying to work with ethernet communication and I started with ''

    STM32F2x7 In-Application Programming (IAP) over Ethernet ''.

    Example works properly but boards must be connected to the ethernet port before that power the board.

    If I plug ethernet cable after powered the board I see ethernet led that blink but I'm not able to connect to the board.

    '' the network is not connected ''