Skip to main content
Stepan Podhorsky
Associate II
Feb 20, 2017 10:34 AM UTC
Solved

STM3220G-EVAL potentiometer

Posted on February 20, 2017 at 11:34

Hello,

I have bought STM3220G-EVAL board (model number MB786) and I am not sure

which ADC module is used for potentiometer RV1 voltage sampling. I have found

that the potentiometer is connected to PF9 pin and I have found in the datasheet

CD00237391 on page 48 that PF9 pin is probably connected to ADC3 module

channel 7. Can anybody confirm to me that it is right? Thank you in advance.

    This topic has been closed for replies.
    Nesrine M_O
    Nesrine M_OBest answer
    Associate
    Feb 20, 2017 1:19 PM UTC
    Posted on February 20, 2017 at 14:19

    Hi

    steven

    ,

    Yes you are right ,A potentiometer RV1 is connected to ADC3of STM32F207IGH6 (PF9 ).

    Please refer to BSP example under the STM32F2 firmware package:

    STM32Cube_FW_F2_V1.4.0\Projects\STM322xG_EVAL\Examples\BSP: This example provides a description of how to use the different BSP drivers.

    -Nesrine-

    2 replies

    Oliver Beirne
    Associate II
    Feb 20, 2017 11:40 AM UTC
    Posted on February 20, 2017 at 12:40

    Hi Stepan

    I have moved your question to the

    https://community.st.com/community/stm32-community/stm32-forum?sr=search&searchId=24ba1400-9c00-466c-be60-80fe7478e201&searchIndex=0

    ‌ where someone should be able to assist you.

    Thanks

    Oli

    Nesrine M_O
    Nesrine M_OBest answer
    Associate
    Feb 20, 2017 1:19 PM UTC
    Posted on February 20, 2017 at 14:19

    Hi

    steven

    ,

    Yes you are right ,A potentiometer RV1 is connected to ADC3of STM32F207IGH6 (PF9 ).

    Please refer to BSP example under the STM32F2 firmware package:

    STM32Cube_FW_F2_V1.4.0\Projects\STM322xG_EVAL\Examples\BSP: This example provides a description of how to use the different BSP drivers.

    -Nesrine-