Skip to main content
robinsm
Associate III
September 2, 2009
Question

STM3210E-EVAL External Data RAM

  • September 2, 2009
  • 2 replies
  • 754 views
Posted on September 02, 2009 at 14:16

STM3210E-EVAL External Data RAM

    This topic has been closed for replies.

    2 replies

    robinsm
    robinsmAuthor
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 13:22

    I cannot inspect that these values are changing while single stepping, Why not? I just see A0000010: -- -- -- -- --...

    *(vu32 *)0xA0000010 = 0x00001011;

    *(vu32 *)0xA0000014 = 0x00000200;

    robinsm
    robinsmAuthor
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 13:22

    I'm trying to use the external RAM as a spot for data with the example code (SRAM_DataMemory). When I single step the code, I get 0xFF's for all the data here in Tab[] after the loop.

    for (Index = 0; Index

    {

    Tab[Index] =Index;

    }

    The linker script is working in ths case but it is not accessing the external memory. In the reset handler I have:

    //#ifdef DATA_IN_ExtSRAM

    /* FSMC Bank1 NOR/SRAM3 is used for the STM3210E-EVAL, if another Bank is

    required, then adjust the Register Addresses*/

    /* Enable FSMC clock */

    *(vu32 *)0x40021014 = 0x00000114;

    /* Enable GPIOD, GPIOE, GPIOF and GPIOG clocks */

    *(vu32 *)0x40021018 = 0x000001E0;

    /* --------------- SRAM Data lines, NOE and NWE configuration ---------------*/

    /*---------------- SRAM Address lines configuration --------*/

    /*---------------- NOE and NWE configuration ---------------*/

    /*---------------- NE3 configuration ------*/

    /*---------------- NBL0, NBL1 configuration ----------------*/

    *(vu32 *)0x40011400 = 0x44BB44BB;

    *(vu32 *)0x40011404 = 0xBBBBBBBB;

    *(vu32 *)0x40011800 = 0xB44444BB;

    *(vu32 *)0x40011804 = 0xBBBBBBBB;

    *(vu32 *)0x40011C00 = 0x44BBBBBB;

    *(vu32 *)0x40011C04 = 0xBBBB4444;

    *(vu32 *)0x40012000 = 0x44BBBBBB;

    *(vu32 *)0x40012004 = 0x44444B44;

    /*---------------- FSMC Configuration -----*/

    /*---------------- Enable FSMC Bank1_SRAM Bank -------------*/

    *(vu32 *)0xA0000010 = 0x00001011;

    *(vu32 *)0xA0000014 = 0x00000200;

    //#endif /*DATA_IN_ExtSRAM*/

    I folowed everything in the readme for the RIDE7 software and even commented the ifdef.

    Are the registers just not set up properly? Any ideas?

    Thanks in advance.

    [ This message was edited by: robinsm on 02-09-2009 14:45 ]