Skip to main content
hauschij
Associate II
May 21, 2009
Question

STM3210B-EVAL USB Speaker Demo

  • May 21, 2009
  • 4 replies
  • 870 views
Posted on May 21, 2009 at 04:56

STM3210B-EVAL USB Speaker Demo

    This topic has been closed for replies.

    4 replies

    hauschij
    hauschijAuthor
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 12:31

    Hallo,

    i have a problem with the speaker demo application. after connecting the STM3210B-EVAL the driver is installed and a device STM32 Speaker is visible. But i can't play sounds on it. Does anybody know why? I use STM3210B-EVAL with Segger J-Link and IAR Embedded Workbench 5.11..works fine.

    plee1
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 12:31

    Did you figure out why the speaker doesn't work? I am having the same problem. Windows detected it but the speaker does not play any sound. Windows doesn't seem to allow the volume to be adjusted for the speaker.

    hauschij
    hauschijAuthor
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 12:31

    JP6 is fitted, an Application with WavePlayer works fine. It use Vista Business with SP1. I get an device called STM32 Speaker, but i cannot play musik on it. The standard format is 8 Bit and 22000 Hz. And it seem that this is not kompatible. I also cannot send an test tone to the device. Message : Seem device not ready...

    jilisegiar
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 12:31

    I tried the same example and it works fine.

    Just check that the JP6:speaker (near the LCD) is fitted.