Skip to main content
dale2
Associate III
January 17, 2008
Question

STM3210B-EVAL shipping with Philips LM75A instead of STLM75 I2C temperature

  • January 17, 2008
  • 2 replies
  • 541 views
Posted on January 17, 2008 at 08:53

STM3210B-EVAL shipping with Philips LM75A instead of STLM75 I2C temperature

    This topic has been closed for replies.

    2 replies

    dale2
    dale2Author
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 12:21

    My STM3210B-EVAL has a Philips (now NXP) LM75A I2C temperature sensor installed instead of the STLM75, which explains why I was getting 2 bonus bits of precision (11 bit instead of 9 bit) in the temperature readings. This gives me 0.125 degree C resoultion instead of 0.5 degree C resolution, which sounds good except that both parts only guarantee +/-2.0 degrees accuracy in the -25C to +100C temperature range.

    The board is marked ''STM3210X-128K-EVAL''. Perhaps it's an earlier revision.

    Thanks,

    Dale Wheat

    16-32micros
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 12:21

    Hi Dale,

    You are right, I have also the same on my board. It seems that The evaluation board manual contains an early revA PCB board.

    STOne-32