Skip to main content
Associate
January 11, 2026
Solved

stm32 with 32 pins with FDCAN but without HSE?

Hello

Im developing a CAN Bus node and with space constrains, so i ve looked in stm32 products and a qnf32 packages looked perfect for example stm32G0B1 has FDCAN. 

The problem...These QFN32 dont expose HSE pins. I just can use HSI with 16 MHz +- 1% wich is not reliable for FDCAN, especially for industrial applications with many nodes. 

I dont understand why the mcu hás 2 FDCAN peripherals if theres no reliable clock to Run them.

Im i missing some thing here? 

At are my alternatives? I now that QFN48 hás HSE, but i dont need só much io and the packages is bigger.

Help here

 

TDK
TDKBest answer
January 11, 2026

> I dont understand why the mcu hás 2 FDCAN peripherals if theres no reliable clock to Run them.

> Im i missing some thing here? 

PC14 can be used as OSC_IN in HSE bypass mode and fed with a clock signal. Use a TCXO rather than a crystal.

TDK_0-1768142506164.png

 

"If you feel a post has answered your question, please click ""Accept as Solution""."

4 replies

TDK
TDKBest answer
January 11, 2026

> I dont understand why the mcu hás 2 FDCAN peripherals if theres no reliable clock to Run them.

> Im i missing some thing here? 

PC14 can be used as OSC_IN in HSE bypass mode and fed with a clock signal. Use a TCXO rather than a crystal.

TDK_0-1768142506164.png

 

"If you feel a post has answered your question, please click ""Accept as Solution""."
ricardosAuthor
Associate
January 11, 2026

Thank you TDK. 

Never did that bypass and never used an TCXO. I'm civil engineer...

Do you have a schematic on how to connect a TCXO to the stm32 MCU with 32 pins? Do I need to connect something to OSC_EN pin?

Thanks a lot

 

TDK
January 11, 2026

A TXCO outputs a clock as a square wave. Connect the output to the OSC_IN pin. That's it. OSC_EN is not needed.

"If you feel a post has answered your question, please click ""Accept as Solution""."