Skip to main content
andrea239955_stm1_st
Associate
February 15, 2010
Question

STM32 Virtual COM problem

  • February 15, 2010
  • 4 replies
  • 879 views
Posted on February 15, 2010 at 15:33

STM32 Virtual COM problem

    This topic has been closed for replies.

    4 replies

    chikos332
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 13:40

    Hi,

    I made a small test and I got much more than the 400Hz, nearly 1000 Hz (for packets of 60-bytes), and it works fine (please check the snapshot in attachments)...

    You may have some special conditions over USART/Data ... ?

    chikos332
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 13:40

    Hi,

    Please, which STM32 chip are you using, on which board and which version of the USB Library ?

    chikos332
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 13:40

    If you are using STM32F103 I don't think you'll have issues.. all issues posted on forum for v3.1.0 are relative to STM32105/7 devices...

    Good luck :)

    andrea239955_stm1_st
    Associate
    May 17, 2011
    Posted on May 17, 2011 at 13:40

    Hi there, sorry for the late i'm answering.

    I'm using the STM32F10X-128K-EVAL with STM32F103VB and the USB library is STM32_USB-FS-Device_Lib_V3.1.0

    I'm planning to run this firmware on a STM32F102R8. Do you think I'm gonna have any problem with that?

    Thanks