Skip to main content
ihouses ihouses
Associate III
Feb 21, 2018 5:04 PM UTC
Solved

STM32 virtual com driver problem

Posted on February 21, 2018 at 18:04

How to remove totally the Virtual COM driver for STM32?

The STlink is working but the virtual com doesn-t work and windows 10 can not find driver to the board.

Since the driver is delivered in a .EXE format I can not indicate windows where the driver is and re-installing the driver or try to auto search doesn't solve the problem.

On the other hand the board is working in another windows machine.

    This topic has been closed for replies.
    ihouses ihouses
    ihouses ihousesBest answer
    Associate III
    Feb 23, 2018 9:48 PM UTC
    Posted on February 23, 2018 at 22:48

    Well, finally I solved the problem selecting manually the driver, as Virtual serial port->st com-port

    Another problem was that I installed the windows 8 driver in a Windows 7 MAchine. Looks like that when the internal FLASH is opening and windows is showing the STM32 drive that virtual serial com port was stopping.

    1 reply

    ihouses ihouses
    ihouses ihousesAuthorBest answer
    Associate III
    Feb 23, 2018 9:48 PM UTC
    Posted on February 23, 2018 at 22:48

    Well, finally I solved the problem selecting manually the driver, as Virtual serial port->st com-port

    Another problem was that I installed the windows 8 driver in a Windows 7 MAchine. Looks like that when the internal FLASH is opening and windows is showing the STM32 drive that virtual serial com port was stopping.