Skip to main content
fing
Associate II
February 25, 2024
Solved

STM32 VCAP pin problem

 Hello,

I have designed a PCB with 3 STM32H725VGT6 MCUs, and assembled them according to my schematic:

schmtc.png

(sorry for this resolution, this is from a converted pdf)

All 3 MCUs are the same, from this schematic.

R5 and R2 are just 0R jumpers to select the boot mode.

At first, ST-Link couldn't find any of them.  When I checked the voltage on the Vcap pin the MCU1 had 1.0008 V at both 2.2uF caps. STLINK still can't find the target. MCU2 and MCU3 had 0.0000V. on the Vcap pins.

All 3 MCUs have their:

- Orientation in the right place

- VDDA / VREF+ connected

- NRST at high 

- 3.3V at all the 100nF decoupling caps

- 2.2uF caps from Murata (ESR < 8 mOhm @ 1 MHz) GRM155R6YA225KE11D

So I was wondering maybe the ICs were bad (which is unlikely considering that they are from Mouser)

I checked the soldering and there were no bridges, but these symptoms are usually caused by some sort of soldering issue.  What else should I check?

 

 

This topic has been closed for replies.
fing
fingBest answer
Associate II
February 29, 2024

Update: 

After some investigation, I found that the main source of the problem was actually caused by incorrect settings in the .ioc file. 

fing_0-1709227217118.png

These are the correct settings for LDO operation.

I can only upload these incorrect settings once. After that, the MCU spits out 0 V on the Vcap pin and it is basically bricked. I have read that if you manually inject 1.3 - 1.4 V on a Vcap pin, you can bring it back to life.

But this was not necessary for my case, because I was able to desolder my BOOT0 jumper and pull it high. Now, ST-Link can detect the MCU, upload and verify the code.

The current consumption went up a little, which meant that the MCU was up and running with 550 MHz. 

 

 

5 replies

TDK
February 25, 2024

Were the PCBs checked electrically before soldering? Who made the boards?

Continuity/resistance test between VDD/GND and VCAP/GND might show some issues.

I agree it's unlikely to be a chip issue--more likely to be a workmanship issue.

"If you feel a post has answered your question, please click ""Accept as Solution""."
fing
fingAuthor
Associate II
February 26, 2024

Yes, JLCPCB made the boards and they passed the flying probe test. 

  • VDD-GND: 3.998 kΩ

MCU1 (which has 1.0008 V on Vcap):

  • VCAP-GND (2.2 uF connected to pin 97): 18.10 kΩ
  • VCAP-GND (2.2 uF connected to pin 44): 18.09 kΩ

MCU2:

  • VCAP-GND (2.2 uF connected to pin 97): 13.00 kΩ
  • VCAP-GND (2.2 uF connected to pin 44): 12.98 kΩ 

MCU3:

  • VCAP-GND (2.2 uF connected to pin 97): 20.68 kΩ
  • VCAP-GND (2.2 uF connected to pin 44): 20.66 kΩ

I might rework the board and maybe replace the caps with fresh ones as well.

ST Technical Moderator
February 25, 2024

 

Best regards

fing
fingAuthor
Associate II
February 26, 2024

Yes, it actually follows the LDO operation, where VDDLDO = VDD. They are powered externally with a power supply giving 3.3 V.

fing
fingAuthorBest answer
Associate II
February 29, 2024

Update: 

After some investigation, I found that the main source of the problem was actually caused by incorrect settings in the .ioc file. 

fing_0-1709227217118.png

These are the correct settings for LDO operation.

I can only upload these incorrect settings once. After that, the MCU spits out 0 V on the Vcap pin and it is basically bricked. I have read that if you manually inject 1.3 - 1.4 V on a Vcap pin, you can bring it back to life.

But this was not necessary for my case, because I was able to desolder my BOOT0 jumper and pull it high. Now, ST-Link can detect the MCU, upload and verify the code.

The current consumption went up a little, which meant that the MCU was up and running with 550 MHz.