STM32 unimplemented interrupts
All of the STM32 devices have unimplemented interrupt numbers, for example on the STM32F767 I am currently using, the last used interrupt MDIOS_IRQn is interrupt number 109.
So is it possible to use the next one, number 110, as a user software interrupt? Obviously there is no peripheral device connected to this interrupt line so there is no danger of a spurious interrupt request, but what's stopping us from defining our own interrupt as
MYOWN_IRQn = 110
And then enabling it and disabling it with NVIC_EnableIRQ(), adding another entry to the interrupt vector table in startup_stm32f767xx.s and using it as a user-defined software interrupt?