Skip to main content
RSy.1
Associate III
June 8, 2020
Question

STM32 UART Interrupt between 2 STM32F103C8 boards.

  • June 8, 2020
  • 8 replies
  • 1855 views

Hello guys good day. I would like to ask for your suggestions regarding the UART interrupt between 2 STM32F103C8 MCUs. I can transmit and receive between 2 MCUs using a single input and output with the use of the IRQHandler. However when I wanted to use the 2nd pin and output I could not transmit and receive anymore. So basically the interrupt is only working for a single inputt/output but for multiple input/output it does not work anymore. I have the codes below:

 // I defined this function before the main
void UARTTX(uint8_t data) 
{
	while(!(USART2 -> SR & USART_SR_TXE));
	USART2 -> DR = data;
}
 
// I defined this function before the main
char UARTRX() 
{
	while(!(USART2 -> SR & USART_SR_RXNE));
	return USART2 -> DR;
}
 
.
.
.
 
 // I enabled these registers before the while loop
USART2 -> CR1 |= USART_CR1_UE; 
USART2 -> CR1 |= USART_CR1_TE;
USART2 -> CR1 |= USART_CR1_RE;
USART2 -> CR1 |= USART_CR1_RXNEIE;
USART2 -> CR1 |= USART_CR1_TXEIE;
 
.
.
.
 
//main code is in the IRQHandler
void USART2_IRQHandler(void) 
{
 HAL_UART_IRQHandler(&huart2);
 {
 //this is first tx output. This code is working only if the second tx output below is not enabled
 if(!HAL_GPIO_ReadPin(BUTTON1_GPIO_Port, BUTTON1_Pin)) 
 {
	USART2 -> DR = 0xFF;																					
 }
 else 
 {
	USART2 -> DR = 0x00;																					
 }
}
	 //this is 2nd tx input and not working 	
//	{
//	 if(HAL_GPIO_ReadPin(BUTTON2_GPIO_Port, BUTTON2_Pin)) 
//	 {
//		USART2 -> DR = 0xF0;																					
//	}
//	else			
//	{
//		USART2 -> DR = 0x0F;																					
//	}
//	}
 
 // this is first rx input and only working if 2nd rx input below is disabled	 
{	
	if(USART2 -> DR == 0xFF) 
	{
		HAL_GPIO_WritePin(LED1_GPIO_Port, LED1_Pin, GPIO_PIN_SET);
	}
	else if(USART2 -> DR == 0x00)
	{
		HAL_GPIO_WritePin(LED1_GPIO_Port, LED1_Pin, GPIO_PIN_RESET);
	}
}
 
  //this is 2nd rx input and is not working
//	{	
//	if(USART2 -> DR == 0xF0) 
//	{
//	HAL_GPIO_WritePin(LED2_GPIO_Port, LED2_Pin, GPIO_PIN_SET);
//	}
//	else if(USART2 -> DR == 0x0F)
//	{
//	HAL_GPIO_WritePin(LED2_GPIO_Port, LED2_Pin, GPIO_PIN_RESET);
//	}
//	}	
}
 
 
 

This topic has been closed for replies.

8 replies

Tesla DeLorean
Guru
June 8, 2020

Read the USART2->DR *ONCE* into a variable, and then inspect the variable

The IRQ will occur ONCE for each byte received, if you need to process a sequence, add a state-machine so you can step through the different states as each byte is received.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
RSy.1
RSy.1Author
Associate III
June 9, 2020

Good day Sir thank you for the answer. I am confused by what you mentioned ONCE. What do you mean by this and how is this written?

Tesla DeLorean
Guru
June 9, 2020

It is a register, it does not behave like RAM. Think of it like a ratcheting sprocket, every time you read the content the machine advances.

{

uint8_t dr = USART2 -> DR; // READ IT ONCE

if(dr == 0xFF) // Compare against the local copy

{

HAL_GPIO_WritePin(LED1_GPIO_Port, LED1_Pin, GPIO_PIN_SET);

}

else if(dr == 0x00)

{

HAL_GPIO_WritePin(LED1_GPIO_Port, LED1_Pin, GPIO_PIN_RESET);

}

}

Also this is really inefficient in a load/store architecture, with volatile register accesses that the compiler/optimize cannot fold

 // I enabled these registers before the while loop

USART2 -> CR1 |= USART_CR1_UE;

USART2 -> CR1 |= USART_CR1_TE;

USART2 -> CR1 |= USART_CR1_RE;

USART2 -> CR1 |= USART_CR1_RXNEIE;

USART2 -> CR1 |= USART_CR1_TXEIE;

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..