Skip to main content
tantankagan
Visitor II
February 4, 2015
Question

Stm32 StdPeriph driver and Eclipse CDT configuration

Posted on February 04, 2015 at 22:57

Hi guys! 

I have a problem with my stm32 discovery board. 

I installed eclipse, gnu arm plugin(version 2.2.1), gcc arm none eabi(4_9-2014q4).

I did not install latest gnu arm plugin because i don't want to use hal_drivers.

After installation, I created new c++ project for stmf4xx std periph driver (toolchain is cross arm gcc).

My problem is that ''When I compile the code (there is no error) and program the board with st-flash, led doesnt blink.

but when i only change to file type .cpp -> .c and program to board led blink.'' 
    This topic has been closed for replies.