Question
STM32 standby wake-up BUG?
STM32 standby mode, standby wake-up pin PA0 and RTC wake up, both can work normally. The problem encountered is: If the wake-up pin PA0 is kept high, when the PA0 high-level hold time exceeds the wake-up time set by the RTC after standby, the chip dies unless the reset button is pressed. Temporarily only test the standby wake-up of the two types of STM32F0 and STM32F4, HAL library.