Skip to main content
mak1308
Associate III
June 24, 2017
Question

STM32 ST-Link Utility - bug?

  • June 24, 2017
  • 3 replies
  • 962 views
Posted on June 24, 2017 at 23:53

I use a debugger of ST-Link and STM32 ST-Link Utility, I try to read 128K of the microcontroller flash-memory from the address 0x08020000. But STM32 ST-Link Utility reads only to the address 0x0802E000 - further the utility shows that memory is empty. But actually in memory there are data. It is a program error?

    This topic has been closed for replies.

    3 replies

    ST Technical Moderator
    June 28, 2017
    Posted on June 28, 2017 at 18:04

    Hi

    G.Marat

    ,

    Which ST-Link Utility version are you using? Is it the latest version?Have you an error message?

    I recommend you to upgrade the ST-Link firwmare through ST-Link utility or this Link

    http://www.st.com/content/st_com/en/products/embedded-software/development-tool-software/stsw-linkhtml

    and tell me if that solve the issue.

    Regards

    Imen

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
    mak1308
    mak1308Author
    Associate III
    June 28, 2017
    Posted on June 28, 2017 at 18:14

    It's latest version - v4.0.0.0.

    I didn't receive the error message.

    Tesla DeLorean
    Guru
    June 28, 2017
    Posted on June 28, 2017 at 18:52

    What part exactly are you using?

    Does the code appear to be at 0x08000000..0x0801FFFF ? Does program/verify indicate an issue?

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..