Question
Stm32 spi with triggered dma
Posted on November 16, 2017 at 16:54
Dear community,
my setup is build on top of stm32f439 and ADS131e4 ADC connected through spi.The adc is set in continuous mode, so it fires an impulse on a pin (DRDY) as soon as a new sample is ready.The sample consists of 15 bytes, and I would likee to read the packet using DMA in double buffer/circular mode.I have tried many solutions without success.My first solution was to simply trigger on the SPI4_RX request.SPI4_RX/TX dma requests are on DMA2 Stream0/1 Channel 4.Once programmed I don't need the tx dma channel, only the rx.Some questions:At this moment I don't want to take care about the double buffer switch so: do I need an interrupt handler for sure?Furthermore, I don't want to transmit: do I need to setup the tx dma channel as well?Final question: If i want to trigger the dma reading from spi can I use a timer channel request?