Skip to main content
DCtech
Associate III
January 6, 2022
Question

STM32 Read Protection And Rx-Tx pins

  • January 6, 2022
  • 1 reply
  • 798 views

I've flash protection level-1 on my stm32f429. When I open the flash protection on my mcu and connect the serial prolific to read and send data under UART. My source code couldnt run. But if I remove the serial prolific's from the pins. And reset the device, device can run. What is the reason ?

This topic has been closed for replies.

1 reply

Peter BENSCH
ST Technical Moderator
February 9, 2022

Your description is not really understandable. Would it be possible for you to post a more detailed description?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.