Skip to main content
Visitor II
June 18, 2025
Question

STM32 Not Detected via ST-Link V2 – Voltage Detected but No Connection

Hi everyone,

I'm having trouble flashing my STM32 microcontroller using an ST-Link V2. STM32CubeProgrammer detects the target voltage, but it fails to connect to the MCU. Here's a summary of my setup and what I've tried:


Setup:

  • Microcontroller: STM32H723ZGT6

  • ST-Link Version: ST-Link V2

  • Flashing Tool: STM32CubeProgrammer (latest version)

  • Connection Interface: SWD

  • Target Voltage Detected: 3.12 V

What I’ve Tried:

  • Verified SWD wiring (SWDIO, SWCLK, GND, VCC)

  • BOOT0 set to 0 (boot from flash)

  • Checked for power on the board

Question:
What else should I try to get the MCU detected? Could this be a clone ST-Link V2 issue, or something else with my MCU or wiring?

Any help is appreciated — thank you!

This topic has been closed for replies.

2 replies

ST Technical Moderator
June 18, 2025

Hello @RShashank and welcome to the Community,

Please have a look at this article which describes tips to fix errors encountered when connecting the STM32 target board to your computer: How to solve connection errors when connecting and programming the STM32 target board

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
TDK
June 18, 2025

Is this a custom board? Show the schematic.

Perhaps also show a picture of the setup with connections between board and programmer.

"If you feel a post has answered your question, please click ""Accept as Solution""."