Skip to main content
Associate III
May 28, 2025 8:08 AM UTC
Question

STM32 N6 Load and Run USART doesn't work

Hi, 

 

I have been trying to deploy the 66GYMAI1 Camera on the STM32 N657X0Q Nucleo board with the Load and Run mode. 

However, there is a problem that I could not solve, which is that the project can not jump from FSBL to APPLI. 

Because I am trying to jump from FSBL to APPLI to print something by USART, but it doesn't work.

I would be grateful if someone could check it.

 

 

 

1 reply

Simon V.
ST Employee
Jan 12, 2026 12:11 PM UTC

Hi,

Which IDE environnement are you using ? Did you try to connect the debug with the software reset mode ?

Regards,

Simon

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.