Skip to main content
JBond.1
Senior
Apr 16, 2020 6:23 PM UTC
Solved

STM32 memory to memory DMA with Timer

Hi, I am trying to do MemToMem DMA operation on Timer input capture.

My code:

#define BufferSize 1000
uint16_t BUFFER_DATA[BufferSize];
 
TIM_HandleTypeDef htim = htim3;
DMA_HandleTypeDef hdma = hdma_tim3_ch4_up;
uint32_t channel = TIM_CHANNEL_4;
uint32_t dma_cc = TIM_DMA_CC4;
uint32_t dma_id_cc = TIM_DMA_ID_CC4;
 
hdma.Init.Direction = DMA_MEMORY_TO_MEMORY;
 
htim.hdma[dma_id_cc]->XferCpltCallback = TIM_DMACaptureCplt;
htim.hdma[dma_id_cc]->XferHalfCpltCallback = TIM_DMACaptureHalfCplt;
htim.hdma[dma_id_cc]->XferErrorCallback = TIM_DMAError;
 
/* Enable the DMA channel */
HAL_DMA_Start_IT(htim.hdma[dma_id_cc], (uint32_t)&GPIOC->IDR, (uint32_t)&BUFFER_DATA[0], BufferSize);
 
/* Enable the TIM Capture/Compare 1 DMA request */
__HAL_TIM_ENABLE_DMA(&htim, dma_cc);
 
/* Enable the Input Capture channel */
TIM_CCxChannelCmd(htim.Instance, channel, TIM_CCx_ENABLE);
 
/* Enable the Peripheral, except in trigger mode where enable is automatically done with trigger */
__HAL_TIM_ENABLE(&htim);

How do I get exact value of (uint32_t)&GPIOC->IDR when timer pin goes low?

Do I need to wait half or full captured interrupt?

Which array element in BUFFER_DATA will be the exact (uint32_t)&GPIOC->IDR value? Or there is no way to tell and I need to loop through BUFFER_DATA and guess?

It seems to me that DMA just copies data to the buffer non-stop and timer just gives me the interupt and thats it, so I need to guess which value do I need to pick from the array, as the timer interupt and DMA are out of sync?

This topic has been closed for replies.
Tesla DeLorean
Tesla DeLoreanBest answer
Guru
Apr 16, 2020 6:53 PM UTC

What STM32 part?

What speed are you clocking/capturing here?

The HT IRQ will fire after BUFFER_DATA[499] has been written TC IRQ after BUFFER_DATA[999]

Yeah, you'll have to come up with a scheme to synchronize, or go fish in the buffer for the signal/pin transitions you want to capture.

The write to the array will beat the TIM3_CC4 IRQ, but you are unlikely to be able to service faster that a few 100 KHz, depending on the core/clock.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..

2 replies

Tesla DeLorean
Tesla DeLoreanBest answer
Guru
Apr 16, 2020 6:53 PM UTC

What STM32 part?

What speed are you clocking/capturing here?

The HT IRQ will fire after BUFFER_DATA[499] has been written TC IRQ after BUFFER_DATA[999]

Yeah, you'll have to come up with a scheme to synchronize, or go fish in the buffer for the signal/pin transitions you want to capture.

The write to the array will beat the TIM3_CC4 IRQ, but you are unlikely to be able to service faster that a few 100 KHz, depending on the core/clock.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
JBond.1
JBond.1Author
Senior
Apr 17, 2020 12:09 PM UTC

Thanks for explanation its a bit more clear now.

I am using STM32F103 with 72Mhz. If I receive data of 1000 uint16_t values each 200ms will this procesor be able to proces it within 200ms?