Skip to main content
Associate III
Jul 30, 2025 6:20 PM UTC
Solved

STM32 MCU to use CAN and USB simultaneously

Hi there 
Is there any stm32 MCU versions that has can run both CAN and USB simultaneously without conflicting with the PB8 boot pin? Also the USB will only be recognized if the PB8 pin is pulled high can i just directly connect it to 3.3v and always keep it on. will that be a problem 

This topic has been closed for replies.
Karl Yamashita
Karl YamashitaBest answer
Principal
Jul 30, 2025 6:55 PM UTC

STM32F105xx, STM32F072 and many more depending on any other requirements. 

 

You can't keep the boot pin tied high else it'll stay in boot mode.

 

If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.CAN Jammer an open source CAN bus hacking toolCANableV3 Open Source

13 replies

Karl Yamashita
Karl YamashitaBest answer
Principal
Jul 30, 2025 6:55 PM UTC

STM32F105xx, STM32F072 and many more depending on any other requirements. 

 

You can't keep the boot pin tied high else it'll stay in boot mode.

 

If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.CAN Jammer an open source CAN bus hacking toolCANableV3 Open Source
Associate III
Jul 30, 2025 6:59 PM UTC

In order to enter the USB the PB8 pins needs to be pulled high. But I can't do it externally is there a way I can pull the pin high just so it enters USB bootloader.

Also i need a smaller package size the ones you mentioned are really big

Karl Yamashita
Principal
Jul 30, 2025 7:17 PM UTC

As far as I can remember, but I could be wrong, 48 pin packages is about the smallest you can go to be able to use both USB and CAN at the same time without any conflicts with shared resources. STM32F042 is another that I use.

The F105 has dual CAN controllers. You didn't give enough info so i threw that out there. 

If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.CAN Jammer an open source CAN bus hacking toolCANableV3 Open Source
Associate III
Jul 30, 2025 7:20 PM UTC

Yeah sorry my bad 48 pin package is good. Thank you @Karl Yamashita . 
I just need to figure one more thing out. How can i enter into USB mode without any external work like pulling the PB8 pin  high using a button. i need it to be just pluggable and i should enter into USB mode . I just need data transmission via USB.

Karl Yamashita
Principal
Jul 30, 2025 7:33 PM UTC

You'll need the software application to send a command to the application FW which will then jump to the built in bootloader. But that's not a good idea as you can brick the device if the FW fails to update, unless you can get to the boot pin.

A better approach is to make a custom bootloader. So even if the application fails to update, you still have the custom bootloader that will still stay in bootloader mode until there is a validate application code in the device.

If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.CAN Jammer an open source CAN bus hacking toolCANableV3 Open Source