Skip to main content
Denis Gottardello
Associate III
May 8, 2017
Question

stm32 lora

  • May 8, 2017
  • 7 replies
  • 1221 views
Posted on May 08, 2017 at 08:48

Hi. I have to study the lora world with a stm32 microcontroller.

For me it is the first approach. Can someone suggest me witch stm32 demo board is the most easy to use in order to learn how lora works?

Can someone suggest me a tutorial?

I need to use lora as sensoristic application.
    This topic has been closed for replies.

    7 replies

    Khouloud GARSI
    ST Employee
    May 8, 2017
    Posted on May 08, 2017 at 11:10

    Hi

    Gottardello.Deni

    ‌,

    The application note

    https://my.st.com/content/ccc/resource/technical/document/application_note/group0/db/8c/4f/5a/95/9e/40/69/DM00346311/files/DM00346pdf/jcr:content/translations/en.DM00346pdf

    may also help you.

    Khouloud.

    Tesla DeLorean
    Guru
    May 8, 2017
    Posted on May 08, 2017 at 14:53

    I'd recommend the 

    B-L072Z-LRWAN1, it is a DISCO board which includes and ST-LINK debugger and the LoRa via a Murata part including an STM32L0 device and the SX1276 radio.

    The USI module is a closed source solution, and the AT modem firmware lacks refinement, the L0 part has significantly less memory, and it uses the older SX1272 radio. I would avoid.

    The NUCLEO and SX127x radio pairings work well.

    The 

    I-CUBE-LRWAN works relatively seamlessly across a number of board combinations, although the code has some significant deficiencies.

    I'm using LoRa as a point-to-point radio link.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Denis Gottardello
    Associate III
    May 30, 2017
    Posted on May 30, 2017 at 16:12

    Many thanks.

    Nesrine M_O
    Associate
    May 30, 2017
    Posted on May 30, 2017 at 16:38

    https://community.st.com/0D50X00009bMM5DSAW

     
    LMI2
    Senior III
    May 30, 2017
    Posted on May 30, 2017 at 21:00

    Who sells the

    B-L072Z-LRWAN1

    , both Digikey and Mouser have zero stock.
    Tesla DeLorean
    Guru
    May 30, 2017
    Posted on May 30, 2017 at 21:36

    They had stock, and sold it. You'll have to back order and wait for deliveries.

    If August isn't appealing, then consider your other options

    Bunch of stock of the P-NUCLEO-LRWAN1 combo board. Qty 222 as I type

    http://www.mouser.com/new/stmicroelectronics/stm-p-nucleo-lrwan1/

     
    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    ST Employee
    May 24, 2018
    Posted on May 24, 2018 at 07:49

    Hello,

    I would like to recommend to you one of our on-line courses dedicated to LoRa.

    It is a recording of our LoRa workshop session from last year.

    Session is free and it requires a free registration.

    More information and access link you can find

    http://www.st.com/content/st_com/en/about/events/events.html/lora-mooc-connect-your-long-range-network-to-the-cloud.html

    .

    Best Regards,

    Artur