STM32-L4 RTC Alarms in Fractional Second Intervals
- January 31, 2018
- 6 replies
- 1763 views
I'm trying to use AN4759 to understand how to configure the RTC alarm for fractional seconds. As an example, I want to trigger an alarm every, say, 10.5 seconds.
Pages 13 and 14 make reference to something that appears to be reference code, but neither the Cube code nor the X-CUBE-RTC code seem to have examples that look like what the application note is asking me to do.
I have tried to make the Cube code here:
\STM32Cube_FW_L4_V1.11.0\Projects\NUCLEO-L476RG\Examples\RTC\RTC_Alarm
do what the app note is asking (I've attached my main.c for reference - it's the only code from the example I've changed other than to use the LSE instead of LSI), but I only appear to be getting integer-second triggers of the alarm. As an example, if I do set my alarm for 10.5 seconds, I appear to be getting alternating 10- and 11-second triggers. It's like on average my trigger is every 10.5 seconds, not individual events. So something is happening, but not what I think should be.
You'll note that I've set salarmstructure.AlarmSubSecondMask = RTC_ALARMSUBSECONDMASK_ALL, which doesn't seem right, but even if I set it to
RTC_ALARMSUBSECONDMASK_NONE it makes no difference - the behavior appears to be the same. Given my prescaler setting of 255 for the LSE, I'd expect to set this to RTC_ALARMSUBSECONDMASK_SS14_8, but that doesn't do anything different either.
Any help would be appreciated.
Thanks,
Scott