Skip to main content
Associate III
Jan 22, 2026 12:13 PM UTC
Question

STM32 internal reference voltage configuration

Hi,
I am working with STM32G491RET6 and currently implementing the ADC. I have a question regarding the ADC reference voltage.

If the external 3.3 V supply is removed from the VREF+ pin and VREFBUF is disabled, does the ADC operate using any internal reference voltage, or will the ADC readings be invalid?

Could someone clarify how the ADC reference behaves in this case?

 

6 replies

waclawek.jan
Super User
Jan 22, 2026 1:24 PM UTC

ADC reference *is* the VREF+ pin, so the ADC readings will be invalid.

JW

Associate III
Jan 22, 2026 1:47 PM UTC

Hi @waclawek.jan ,
So there is no internal reference voltage to read ADC inputs, right?

mƎALLEm
ST Technical Moderator
Jan 22, 2026 1:49 PM UTC

No reference voltage: ADC not working as expected-> reading is invalid and there is no recovery mechanism to detect the unavailability if Vref

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
Associate III
Jan 22, 2026 1:52 PM UTC

Hi @mƎALLEm ,
I am confused with the internal reference voltage VREFINT, can I use that as a reference if no external VREF+ is provided?

mƎALLEm
ST Technical Moderator
Jan 22, 2026 1:57 PM UTC

I've already answered that question in this thread.

You can use VREFBUF instead of the external VREF voltage but you need to enable VREFBUF in your application. and you should disconnect any other external VREF source and connect an external decoupling capacitor.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
TDK
Jan 22, 2026 2:25 PM UTC

VREFINT has nothing to do with the ADC. It is not a voltage reference for the ADC.

"If you feel a post has answered your question, please click ""Accept as Solution""."