Skip to main content
sukrubahadirarslan
Associate II
December 18, 2013
Question

STM32 I2C problem

  • December 18, 2013
  • 2 replies
  • 841 views
Posted on December 18, 2013 at 19:46

hello.

I want to communicate with sensör with I2C.

First I must send the sensor register address to sensor.

And then I receive the data from this sensor register.

So first I configure I2C peripheral as master transmitter.

Can I change the master transmitter to master receiver without generating stop condition ? 

I mean, I write this code : 

I2C_GenerateSTART(I2C1,ENABLE);

I2C_GetFlagStatus(I2C1,I2C_FLAG_SB);

while(I2C_GetFlagStatus(I2C1,I2C_FLAG_MSL)==RESET);

I2C_Send7bitAddress(I2C1,MPU6050_Default_Address,I2C_Direction_Transmitter);

while(I2C_GetFlagStatus(I2C1,I2C_FLAG_TRA)==RESET);

while(I2C_GetFlagStatus(I2C1,I2C_FLAG_ADDR)==RESET);

I2C_GetFlagStatus(I2C1,I2C_FLAG_ADDR); 

 I2C_GetFlagStatus(I2C1,I2C_FLAG_MSL); // read sr2 . clear ADDR bit.

I2C_SendData(I2C1,Gyrox_Data_MSB8_Register_Address);

while(I2C_GetFlagStatus(I2C1,I2C_FLAG_TXE)==RESET);

// Should I generate a STOP condition here ? or Can I resume like this ? :

I2C_GenerateSTART(MPU6050_I2C, ENABLE);

I2C_Send7bitAddress(MPU6050_I2C, slaveAddr, I2C_Direction_Receiver);

...

thanks for your help

    This topic has been closed for replies.

    2 replies

    chen
    Associate II
    December 19, 2013
    Posted on December 19, 2013 at 10:56

    Hi

    I am not going to debug you code.

    ''Can I change the master transmitter to master receiver without generating stop condition ?''

    Yes.

    It is called a 'repeated start condition'.

    The full I2C spoecification :

    http://www.nxp.com/documents/user_manual/UM10204.pdf

    Sadly, it is long winded and goes on about lots of stuff (like ultra high speed) that is not relevant to you.

    There are loads of information about I2C on the WEB.

    sukrubahadirarslan
    Associate II
    December 20, 2013
    Posted on December 20, 2013 at 14:36

    Thanks a lot. 

    this document is very good.

    I have one more different question.

    I read in datasheet that : I must clearADDR bit after address transmission.

    In this code I monitor ADDR bit like this : 

    while(I2C_GetFlagStatus(I2C1,I2C_FLAG_ADDR)==RESET);

    When ADDR bit is set , ADDR bit is clear in this line ? or 

    Should I write this code like this for clearing the ADDR bit ? 

    while(I2C_GetFlagStatus(I2C1,I2C_FLAG_ADDR)==RESET);

    I2C_GetFlagStatus(I2C1,I2C_FLAG_ADDR) ----> t

    his line is required ???

    sorry about my english .

    thanks again.