Skip to main content
valentin2399
Visitor II
November 29, 2016
Question

STM32 HAL I2C Problem

Posted on November 29, 2016 at 10:56

Hello everyone,

for my current project I am trying to communicate with my STM32F407 Discovery board via I2C. I want to poll different data from it using an Arduino board, similar to a sensor I have. The sensor polling already works and is as follows: I send send the address with a write bit, then a register I want the value from, then I send the slave address once more, only this time with a read bit. I then expect a float.

So far I have managed to detect my STM using a scanner I implemented. I have trouble moving on from there though mainly because I do not understand the driver description of the HAL library I suppose.

My code:

//I2C Initialization

I2C_HandleTypeDef hi2c1;

void InitializeI2C1()

{

__I2C1_CLK_ENABLE();

hi2c1.Instance             = I2C1;

hi2c1.Init.AddressingMode  = I2C_ADDRESSINGMODE_7BIT;

hi2c1.Init.ClockSpeed      = 100000;

hi2c1.Init.DualAddressMode = I2C_DUALADDRESS_DISABLED;

hi2c1.Init.DutyCycle       = I2C_DUTYCYCLE_2;

hi2c1.Init.GeneralCallMode = I2C_GENERALCALL_DISABLED;

hi2c1.Init.NoStretchMode   = I2C_NOSTRETCH_DISABLED;

hi2c1.Init.OwnAddress1     = 0x25<<1;

if (HAL_I2C_Init(&hi2c1) != HAL_OK)

{

Error_Handler();

}

HAL_NVIC_SetPriority(I2C1_EV_IRQn,0,1);

HAL_NVIC_EnableIRQ(I2C1_EV_IRQn);

__GPIOB_CLK_ENABLE();

GPIO_InitTypeDef GPIO_InitStructure;

GPIO_InitStructure.Pin       = GPIO_PIN_6|GPIO_PIN_7;

GPIO_InitStructure.Mode      = GPIO_MODE_AF_OD; //

GPIO_InitStructure.Speed     = GPIO_SPEED_HIGH;

GPIO_InitStructure.Pull      = GPIO_PULLUP;

GPIO_InitStructure.Alternate = GPIO_AF4_I2C1;

HAL_GPIO_Init(GPIOB, &GPIO_InitStructure);

HAL_I2C_EnableListen_IT(&hi2c1);

}

extern ''C'' void I2C1_EV_IRQHandler()

{

HAL_I2C_EV_IRQHandler(&hi2c1);

}

// My code for the (already functioning) detect:

void HAL_I2C_AddrCallback(I2C_HandleTypeDef * hi2c, uint8_t TransferDirection, uint16_t AddrMatchCode)

{

}

void HAL_I2C_ListenCpltCallback(I2C_HandleTypeDef * hi2c)

{

HAL_I2C_EnableListen_IT(&hi2c1);

}

void main()

{

InitializeI2C1();

while(1)

{

}

}

For the next step I am just sending the 1 byte register address. So, on the STM board the question is: what do I do? I assume I still have to have the HAL_I2C_EnableListen_IT, otherwise no transmission will take place, correct? Where in the code should I implement the HAL_I2C_Slave_Receive_IT because if I do it in the HAL_I2C_AddrCallback, the I2C line gets help up and nothing works anymore. The same applies if I put it in my main...

Thank you for your time.
    This topic has been closed for replies.

    1 reply

    Walid FTITI_O
    Visitor II
    November 30, 2016
    Posted on November 30, 2016 at 14:47

    Hi  BesenSelqnin, 

    I recommend you to have a look to the ready-to-use example inside the STM32CubeF4 ''I2C_TwoBoards_ComIT''  at this path  STM32Cube_FW_F4_V1.14.0\Projects\STM32F4-Discovery\Examples\I2C\I2C_TwoBoards_ComIT

    See how the I2C state machine is implimented to send and receive data in interruption mode.

    -Hannibal-