STM32 HAL flash interrupts
I'm working with the STM32L152. I'm finding that after my code runs for some time, during a write attempt to the EEPROM,
the flash controller status register shows the WRPERR and SIZERR bits set, which causes the write to be aborted. This is happening
somewhere before the write is attempted.
I'd like to use the error interrupt to find out where the bits are being set. However, the only HAL function I see that uses interrupts
is HAL_FLASH_Program_IT(). Our code is using HAL_FLASHEx_DATAEEPROM_Program(), which calls functions that do not have interrupt based equivalents
(FLASH_DATAEEPROM_ProgramWord(), _ProgramByte(), etc).
Are there any equivalent functions that use the flash interrupts I can use to find the source of the errors. Thanks.
Lee