Skip to main content
wjian.2
Associate III
August 12, 2023
Question

stm32 h747 uart8 hal_uart_init wrong

  • August 12, 2023
  • 3 replies
  • 1643 views

If when i use hal_uart_init(&huart8) get result Details:HAL_ERROR Default:HAL_ERROR,Decimal:1,Hex:0x1,Binary:1,Octal:01.When i use step into ,reach at final while(sets-- !=0u)and no more what does this mean ? how could i solve this problem?

wjian2_0-1691841082867.png

 

static void MX_USART8_UART_Init(void)
{

/* USER CODE BEGIN USART1_Init 0 */

/* USER CODE END USART1_Init 0 */

/* USER CODE BEGIN USART1_Init 1 */

/* USER CODE END USART1_Init 1 */
huart8.Instance = UART8;
huart8.Init.BaudRate = 115200;
huart8.Init.WordLength = UART_WORDLENGTH_8B;
huart8.Init.StopBits = UART_STOPBITS_1;
huart8.Init.Parity = UART_PARITY_NONE;
huart8.Init.Mode = UART_MODE_TX_RX;
huart8.Init.HwFlowCtl = UART_HWCONTROL_NONE;
huart8.Init.OverSampling = UART_OVERSAMPLING_16;
huart8.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE;
huart8.Init.ClockPrescaler = UART_PRESCALER_DIV1;
huart8.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT;

if (HAL_UART_Init(&huart8) != HAL_OK)
{
Error_Handler();
}

This topic has been closed for replies.

3 replies

Pavel A.
August 12, 2023

The GDB debugger is unable to step through SCB_EnableDCache and other SDB...Cache inline functions. This is a known issue, I don't know the exact reason. Just do not step into these functions, leave them alone.

This is not related to your UART problem. If in doubt, just do not enable the caches yet.

Are there other issues with your UART?

wjian.2
wjian.2Author
Associate III
August 12, 2023

so what is the posible reason for hal_uart_init(&huart8) get HAL_ERROR?

Tesla DeLorean
Guru
August 12, 2023

All the source is available, review the exit paths.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..