Skip to main content
jamie23
Associate II
January 7, 2016
Question

STM32 GPIO not Hi-Z during standby?

  • January 7, 2016
  • 0 replies
  • 477 views
Posted on January 07, 2016 at 12:14

Hi, similar (but different) issue to a previous posting of mine.

I am seeing PA1 on an STM32F205 get driven low during standby after __WFI()

I was expecting all GPIO to go Hi-Z during standby apart from the pins detailed in the datasheet (and SWD/JTAG pins when sleep-debugging is enabled).

I thought it might be an issue with clocks being disabled before sleep so I am now manually changing PA1 to an input before standby (it's used as an output in my design). There is an external 10K pull-up on PA1, but it still gets driven to 0v during standby.

If I dont enable debug sleep, then the pin behaves as expected, but if I call

DBGMCU_Config(DBGMCU_STANDBY, ENABLE);

before standby, I see this behaviour.

Thanks in advance for any tips.

Jamie.
    This topic has been closed for replies.