Skip to main content
Associate III
June 24, 2024
Question

stm32 GPIO Configuaration

I am using a pin to Switch on the power supply once the MCU is powered.When powering up the MCU I am getting a Glitch before it turns on the MC

GPIO configuaration is given below. For every output I am getting a glich before it SET from RESET   Can anyone help 

 

 

static void MX_GPIO_Init(void)
{
 GPIO_InitTypeDef GPIO_InitStruct = {0};
/* USER CODE BEGIN MX_GPIO_Init_1 */
/* USER CODE END MX_GPIO_Init_1 */

 /* GPIO Ports Clock Enable */
 __HAL_RCC_GPIOB_CLK_ENABLE();
 __HAL_RCC_GPIOC_CLK_ENABLE();
 __HAL_RCC_GPIOA_CLK_ENABLE();

 /*Configure GPIO pin Output Level */
 HAL_GPIO_WritePin(GPIOB, NFC_Pin|SHN_Pin|RL_A_Pin|LedR_Pin
 |DPS_Pin, GPIO_PIN_RESET);

 /*Configure GPIO pin Output Level */
 HAL_GPIO_WritePin(GPIOA, RL_B_Pin|DA_TX_Pin|LedG_Pin, GPIO_PIN_RESET);

 /*Configure GPIO pin : NFC_Pin */
 GPIO_InitStruct.Pin = NFC_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
 GPIO_InitStruct.Pull = GPIO_PULLUP;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 HAL_GPIO_Init(NFC_GPIO_Port, &GPIO_InitStruct);

 /*Configure GPIO pins : RL_B_Pin LedG_Pin */
 GPIO_InitStruct.Pin = RL_B_Pin|LedG_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);

 /*Configure GPIO pin : PA4 */
 GPIO_InitStruct.Pin = GPIO_PIN_4;
 GPIO_InitStruct.Mode = GPIO_MODE_INPUT;
 GPIO_InitStruct.Pull = GPIO_PULLUP;
 HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);

 /*Configure GPIO pin : Mains_Pin */
 GPIO_InitStruct.Pin = Mains_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_INPUT;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 HAL_GPIO_Init(Mains_GPIO_Port, &GPIO_InitStruct);

 /*Configure GPIO pin : SHN_Pin */
 GPIO_InitStruct.Pin = SHN_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_OD;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 HAL_GPIO_Init(SHN_GPIO_Port, &GPIO_InitStruct);

 /*Configure GPIO pins : RL_A_Pin LedR_Pin */
 GPIO_InitStruct.Pin = RL_A_Pin|LedR_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);

 /*Configure GPIO pin : DA_TX_Pin */
 GPIO_InitStruct.Pin = DA_TX_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
 GPIO_InitStruct.Pull = GPIO_PULLDOWN;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 HAL_GPIO_Init(DA_TX_GPIO_Port, &GPIO_InitStruct);

 /*Configure GPIO pin : LIVE_SENSE_Pin */
 GPIO_InitStruct.Pin = LIVE_SENSE_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_INPUT;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 HAL_GPIO_Init(LIVE_SENSE_GPIO_Port, &GPIO_InitStruct);

 /*Configure GPIO pin : DPS_Pin */
 GPIO_InitStruct.Pin = DPS_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
 HAL_GPIO_Init(DPS_GPIO_Port, &GPIO_InitStruct);

 /*Configure GPIO pin : DA_RX_Pin */
 GPIO_InitStruct.Pin = DA_RX_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_IT_FALLING;
 GPIO_InitStruct.Pull = GPIO_PULLDOWN;
 HAL_GPIO_Init(DA_RX_GPIO_Port, &GPIO_InitStruct);

 /* EXTI interrupt init*/
 HAL_NVIC_SetPriority(EXTI4_15_IRQn, 0, 0);
 HAL_NVIC_EnableIRQ(EXTI4_15_IRQn);

 

 

This topic has been closed for replies.

3 replies

mƎALLEm
ST Technical Moderator
June 24, 2024

Hello,

I am using a pin to Switch on the power supply once the MCU is powered.When powering up the MCU I am getting a Glitch before it turns on the MC

 

 This statement is not clear: "Switch on the power supply" of what? and what "MC" stands for?

Also what is the pin that "switches the power supply" in your code? and what is the exact GPIO pin used for that purpose as in your code you've used definitions.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
Andrew Neil
Super User
June 24, 2024

@meena wrote:

I am using a pin to Switch on the power supply once the MCU is powered.


Show the schematic of how you're doing that.

Remember that you have no control of the state of the GPIO pin in the time between the MCU starting, and your code reaching the point at which it configures the pin ...

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Tesla DeLorean
Guru
June 24, 2024

If you want to control the state of a pin out of reset, the normal method is to use an external pull-up/down resistor

And for things that are safety critical, probably two pins at different states to provide some level of interlock.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..