What, exactly, ''doesn't work''? In what way does it ''not work''?''help me please'' It's hard to help when you don't say what the actual problem is!
A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
There are specific requirements regarding the address used as a vector table location, and there will still need to be a primary vector table from which to boot.
You might need to modify your startup.s or crt0_gnu.s, to achieve your goals cleanly and efficiently.
Tips, Buy me a coffee, or three.. PayPal VenmoUp vote any posts that you find helpful, it shows what's working..
We'll I'm pretty sure that if you are executing ANY code from FLASH (ie outside your IRQ) it's going to be stalling the pipeline in a non-interruptable way.
The quickest way to test that is to make a small foot-print demo that runs completely in RAM.
Tips, Buy me a coffee, or three.. PayPal VenmoUp vote any posts that you find helpful, it shows what's working..
My vectors table is in SRAM, my IRQHandler is in SRAM and is executed when data arrives during the execution of FLASH_Erase but it is as if USART1 not working!
I do not know what else to try!
This is myUSART1_ IRQHandler INRAM void INRAM_USART1_IRQHandler(void) { uint16_t reg; if ((USART1->SR & USART_FLAG_RXNE)) { // Réemission de la donnée USART1->DR = USART1->DR; Test=32; } if ((USART1->SR & USART_FLAG_IDLE)) { // Ligne IDLE // Clear IT pending reg = USART1->SR; reg = USART1->DR; IndexRcp = ID_ADR_DST; EnEcoute = TRUE; LgLSB = FALSE; } if ((USART1->SR & USART_FLAG_LBD)) { // LIN BREAK detection // Clear IT pending USART1->SR &= (uint16_t)~USART_FLAG_LBD; // La carte est transparente, le BREAK est envoyé immédiatement USART1->CR1 |= CR1_SBK_Set; Test=33; } if ((USART1->SR & USART_FLAG_ORE)) { // Error interrupt // OverRun Error interrupt UARTErreur |= USART_FLAG_ORE; reg = USART1->SR; reg = USART1->DR; } if ((USART1->SR & USART_FLAG_NE)) { // Noise Error interrupt UARTErreur |= USART_FLAG_NE; // Clear IT pending reg = USART1->SR; reg = USART1->DR; } }
You will need to copy the entire vector table into RAM, as well as the as having the one you booted from. The IRQ routines need to be in RAM, along with any library code it calls/touches. As any access to FLASH during the write/erase functions will block processor execution.
Tips, Buy me a coffee, or three.. PayPal VenmoUp vote any posts that you find helpful, it shows what's working..